Back to Main Menu

Environmental Cost

Note:This is a licensed feature. To have this feature enabled, please contact ams-assetic-support.si@siemens.com

On the Environmental Cost tab, the cost per unit for the Environmental Parameters added in the template can be configured, and a cost chart is shown.

 

To configure the costing, users can double-click on the relevant field in the Environmental Cost grid.

 

These values are then used by Predictor's calculations when relevant reports are run.